Generate a partial program
Generate Partial Program
exports a Logix Designer XML file (L5X) that can be imported into the Logix Designer
as a program.To generate a partial program
- In thePreviewpane, expandControllers, expand the controller object, right-click the program object to export and then clickGenerate Partial Program.TheLogix Code Generationdialog displays.
- (optional) To rename the file click in theSave Asfield. The text box becomes editable and the current file name is highlighted. Type the new file name.
- Verify that theGenerateandACM Project Datacheckboxes are selected.
- Select theOverwrite Existingcheckbox if you want to replace an earlier file with the same name.TheCreate ACDoption is disabled. Partial program and routine items can only be generated using .L5X files.
- InSave Path, type the path where the exported files should be saved or use the default path:C:\Users\<username>\AppData\Local\Rockwell Automation\Application Code Manager\OutputReplace the <username> variable with your current Windows username.
- ClickGenerate.The files are generated. A status message displays when completed.
- (optional) ClickOpen Folderto open the file explorer to the file location.
Provide Feedback