Detach a controller
If a controller is updated using an ACD or L5X file, then the controller will maintain an
attachment to that file. The next time ACM is started, the ACM application will attempt to
establish a connection to the file. Depending on file systems, file size, and file location
establishing a connection to an ACD or L5X file may take more time than expected. If needed,
the ACM application can detach the file from the controller.
To detach from an ACD/L5X file
- In thePrevieworClass Viewpane, right-click the controller to which the file is attached to and then selectDetach from ACD/L5X.
Provide Feedback