Modify step tags or sequencing parameters using the Sequence Parameters Control
Select a step tag or sequencing parameter from the list on the Sequence Parameters Control to modify, disable or enable, force evaluation of, or view more information about the step tag or sequencing parameter.
Tip: | To modify settings for tags and parameters, the external value for the tags and parameters must be set to Read/Write . Use the Tag Editor in the Logix Designer application to change the external value for a tag or parameter. |
To modify a tag or parameter
- Select the tag or parameter.
- In theValuebox, type the new value for the tag or parameter.
- To disable or enable a tag or parameter, selectExpressionand then selectDisable ExpressionorEnable Expression. When you disable a tag or parameter, the disabled icon
appears in the
Expressionbox. To re-enable a disabled tag or parameter, selectExpressionand then selectEnable Expression. When you re-enable a disabled expression, the disabled icon disappears from theExpressionbox. - To force evaluation of a tag or parameter, selectExpressionand then selectForce Evaluation. TheForce Evaluationbutton is disabled when any of these are true:
- TheEquipment Sequenceis in the IDLE state.
- The controller is in Program mode.
- TheEquipment Sequenceor its assigned task is disabled.
- TheEquipment Sequenceis unscheduled.TIP:If a description is truncated, hover over the description to see the full description in a tool-tip.
Provide Feedback