Configure the Sequence Parameters Control

To configure the
Sequence Parameters Control,
you need to customize several settings in the
Property Panel
for the control.
You can configure the
Sequence Parameters Control
to communicate with a controller, to use VBA scripting, or (to) change display options.
Prerequisites
  • Open the
    FactoryTalk View
    Site Edition (SE) application.
  • Open a display that contains the
    Sequence Parameters Control
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal