Configure the Sequence Parameters control to communicate with a controller

To configure the Sequence Parameters Control:
  1. In the display window, right click the
    Sequence Parameters Control
    .
  2. Select
    Property Panel
    .
  3. Select the
    Properties
    tab.
  4. In the
    ControllerPath
    property text box, enter the path for the controller.
  5. In the
    ControllerShortcut
    property text box, enter the RSLinx Enterprise device shortcut name to the controller
  6. In the
    DataServerPath
    property text box, enter the FactoryTalk path to the RSLinx Enterprise data server.
  7. In the
    SequenceName
    property text box, enter the name of the Equipment Sequence.
  8. In the
    SeqMgrServerPortNumber
    property text box, enter the port number that was defined during the installation of the server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal