Configure the Sequence Summary Control to communicate with a controller

To configure the Sequence Summary Control to communicate with a controller
  1. In the display window, right-click the
    Sequence Summary Control
    .
  2. Select
    Property Panel
    .
  3. Select the
    Properties
    tab.
  4. In the
    ControllerPath
    property text box, enter the FactoryTalk Linx Harmony path for the controller.
    For example:
    AB_ETH-1\99.99.99.99\Backplane\0
  5. In the
    ControllerShortcut
    property text box, enter the FactoryTalk Linx device shortcut name to the controller.
  6. In the
    DataServerPath
    property text box, enter the FactoryTalk path to the FactoryTalk Linx data server. This can be a relative path or an RNA path
    For example:
    MyProject/MyArea/
    - or -
    RNA://$Local/MyProject
  7. In the
    SeqMgrServerPortNumber
    property text box, enter the port number that was defined during the installation of the
    SequenceManager
    Server service and the ActiveX controls. Default value is 7452.
  8. Close the
    Property Panel
    window.
  9. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal