Configure the Sequence Summary Control
To configure the
Sequence Summary Control
to communicate with a controller or to use VBA, you need to customize several settings in the Property Panel
for the control. You can also customize display options.Prerequisites
- Open theFactoryTalk ViewSite Edition (SE) application.
- Open a display that contains theSequence Summary Control.
Provide Feedback