Sequence Parameter Control events

The
Sequence Parameter Control
has the following event that can be used by a client in runtime.
Name
Description
everyTagConnectedChanged
Occurs whenever the value of the IsEveryTagConnected property changes. The event has a single Boolean parameter that is the current IsEveryTagConnected property value.
liveDataConnectedChanged
Occurs whenever the value of the IsLiveDataConnected property changes. The event has a single Boolean parameter that is the current IsLiveDataConnected property value.
seqMgrServerConnectedChanged
Occurs whenever the value of the IsSeqMgrServerConnected property changes. The event has a single Boolean parameter that is the current IsSeqMgrServerConnected property value.
seqMgrServerConnectedBackupChanged
Occurs whenever the value of the IsSeqMgrServerConnectedBackup property changes. The event has a single Boolean parameter that is the current IsSeqMgrServerConnectedBackup property value.
seqMgrServerToControllerConnectedChanged
Occurs whenever the value of the IsSeqMgrServerToControllerConnected property changes. The event has a single Boolean parameter that is the current IsSeqMgrServerToControllerConnected property value.
seqMgrServerToControllerConnectedBackupChanged
Occurs whenever the value of the IsSeqMgrServerToControllerConnectedBackup property changes. The event has a single Boolean parameter that is the current IsSeqMgrServerToControllerConnectedBackup property value.
sequenceStateChanged
Occurs whenever the value of the SelectedSequenceState property changes. The event has a single integer parameter that is the current SelectedSequenceState property value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal