The
SequenceManager
Controls

The
SequenceManager
ActiveX Controls sequences a series of
Equipment Phase
s to the Control Logix platform. The operator views and interacts with the
Equipment Sequence
s downloaded to a Logix controller through three types of controls:
  • Sequence Detail Control
    The
    Sequence Detail Control
    provides the operator with a detailed view of an
    Equipment Sequence
    , including its chart structure, steps, and transitions. The runtime status of the sequence program and its sequence elements are also shown. The operator can command the
    Equipment Sequence
    from this control.
  • Sequence Summary Control
    The
    Sequence Summary Control
    displays the sequence program status for each of the
    Equipment Sequence
    s downloaded to the controller. The
    Sequence Summary Control
    also allows the operator to view and command a selected
    Equipment Sequence
    .
  • Sequence Parameters Control
    The
    Sequence Parameters Control
    displays a table of all sequencing parameters and step tags of a specified
    Equipment Sequence
    , and allows the operator to command a selected sequencing parameter or step tag. To refine the display, configure the table to filter the displayed information.
    Sequence Parameters Control validates the value so it is within the configured Min and Max range.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal