Sequence Parameters Control runtime data

Use Sequence Parameters Control to make data available for VBA programmers at runtime. The following properties are read-only assigned data.
Property Name
Description
Read Only
Value Type
IsEveryTagConnected
Displays whether every tag is connected to the ActiveX control.
True = -1 and False = 0.
Default value: -1
Yes
Integer
IsLiveDataConnected
Displays whether the live data server is connected to the ActiveX control.
True = -1 and False = 0.
Default value: 0
Yes
Integer
IsSeqMgrServerConnected
Displays whether the
SequenceManager
Server Service application is connected to the ActiveX control.
True = -1 and False = 0.
Default value: 0
Yes
Integer
IsSeqMgrServerConnectedBackup
Displays whether the backup
SequenceManager
Server Service application is connected to the ActiveX control.
True = -1 and False = 0.
Default value: 0
Yes
Integer
IsSeqMgrServerToControllerConnected
Displays whether the
SequenceManager
Server Service application is connected to the controller.
True = -1 and False = 0.
Default value: 0
Yes
Integer
IsSeqMgrServerToControllerConnectedBackup
Displays whether the backup
SequenceManager
Server Service application is connected to the controller.
True = -1 and False = 0.
Default value: 0
Yes
Integer
SequenceState
Displays the state value of the selected Equipment Sequence.
Yes
String
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal