Configure the Sequence Detail Control display options

To configure the Sequence Detail Control display options
  1. Right-click the
    Sequence Detail Control
    in the display window.
  2. Select
    Property Panel
    .
  3. (optional) In the
    AutoScroll
    property text box, select
    True
    .
  4. (optional) In the
    CommandButtonLocation
    property text box, choose the location for the
    Equipment Sequence
    command buttons.
  5. (optional) In the
    ShowCommandButtons
    property text box, select
    True
    to display the command buttons.
  6. (optional) In the
    ShowStatusBar
    property text box, select
    True
    to display the status bar.
  7. (optional) In the
    TouchPointerSize
    property text box, select an option to auto-size, decrease, or increase the size of buttons.
  8. Close the
    Property Panel
    window.
  9. Select
    Save
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal