Sequence Parameters Control property settings
The
Sequence Parameters Control
has the following properties that are configurable in the Property Panel of the control in the FactoryTalk View SE
application.Property name | Description | Read only | Value type |
---|---|---|---|
AutoLoad | Determines if the sequence chart is loaded automatically after the FactoryTalk View SE runtime starts. | No | Boolean |
Column1Content | Determines what content is displayed in Column 1. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
Column2Content | Determines what content is displayed in Column 2. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
Column3Content | Determines what content is displayed in Column 3. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
Column4Content | Determines what content is displayed in Column 4. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
Column5Content | Determines what content is displayed in Column 5. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
Column6Content | Determines what content is displayed in Column 6. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
Column7Content | Determines what content is displayed in Column 7. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
Column8Content | Determines what content is displayed in Column 8. | No | 1 – Usage 2 – Value 3 – Initial Value 4 – Initialize As Valid 5 – Expression 6 – Data Type 7 – Description 8 – Engineering Unit 9 – Not Used |
ControllerPath | Controller path of the Equipment Sequence . This path is specific to the workstation on which the SequenceManager Server is communicating with is located.Path Example: AB_ETH-1\99.99.99.99\Backplane\0 | No | String |
ControllerShortcut | FactoryTalk Linx device shortcut to the controller. Default Value: MY_CONTROLLER | No | String |
CurrentFilter | Determine which filter is currently being used. Default value: 0 – All | No |
|
DataServerPath | The FactoryTalk View SE path to the FactoryTalk Linx Data Server.Example Path: My Project/MyArea -or- RNA://$Local/MyProject/ | No | String |
IsEveryTagConnected | Displays whether every tag is connected to the ActiveX Control. Default value: True | Yes | Boolean |
IsLiveDataConnected | Displays whether the live data server is connected to the ActiveX Control. Default value: False | Yes | Boolean |
IsSeqMgrServerConnected | Displays whether the primary SequenceManager Server is connected to the ActiveX Control. Default value: False | Yes | Boolean |
IsSeqMgrServerConnectedBackup | Displays whether the backup SequenceManager Server is connected to the ActiveX Control. Default value: False | Yes | Boolean |
IsSeqMgrServerToControllerConnected | Displays whether the primary SequenceManager Server is connected to the controller. Default value: False | Yes | Boolean |
IsSeqMgrServerToControllerConnectedBackup | Displays whether the backup SequenceManager Server is connected to the controller. Default value: False | Yes | Boolean |
LoadTable | Determines if the table is loaded to the window. | No | Boolean |
SelectedSteps | Names of the selected steps. If multiple step names are entered, each step name must be separated by a comma from other step names. | No | String |
SeqMgrServerAddress | The IP address of the workstation hosting the primary SequenceManager Server. | No | String |
SeqMgrServerAddressBackup | The IP address of the workstation hosting the backup SequenceManager Server. | No | String |
SeqMgrServerPortNumber | The port number of the workstation hosting the SequenceManager Server. Default value: 7452 | No | String |
SequenceName | Name of the Equipment Sequence that the chart loads if a load is initiated using the AutoLoad or LoadChart properties. | No | String |
SequenceState | Displays the state value of the displayed Equipment Sequence . | Yes | Integer |
ShowFilter | Determines if the filter box is shown. | No | Boolean |
ShowSequenceHeader | Determines if the sequence header is shown. | No | Boolean |
ShowStatusBar | Determines if the status icons are shown. | No | Boolean |
SortField | Determines which column the table is sorted on. | No | 0 – ParameterName 1 – ParameterUsage 2 – ParameterValue 3 – ParameterInitialValue 4 – ParameterInitializeAsValid 5 – ParameterExpression 6 – ParameterDataType 7 – ParameterDescription 8 – ParameterEngineeringUnit |
SortOrder | Determines which order the table is sorted, ascending, or descending. | No | 0 – Ascending 1 – Descending |
TouchPointerSize | Determines the size of the command buttons and the height of the fields in the header and footer areas. | No | 1 – Large 2 - Small |
Provide Feedback