Sequence Parameters Control table columns

This table describes the columns in the Sequence Parameters Control list. The Parameters Control list includes all the step tags and sequence parameters in an
Equipment Sequence
.
Use the
Filter
setting to limit the types of tags and parameters that are included in the list. Select the column headers to sort the list alphabetically to group similar tags and parameters.
Column
Description
Name
The name of the step tag or sequencing parameter.
Usage
The usage type of the step tag or sequencing parameter. Usage types include
Step input
and
Step output
for step tags, and
Input
and
Output
for sequencing parameters.
Value
The current value of the step tag or sequencing parameter. Values can be edited when the
External Access
for the tag or parameter is set to
Read/Write
. Use the Tag Editor in the
Logix Designer
application to change the external value for a tag or parameter. Sequence Parameters control validates the value so it is within the configured Min and Max range.
Initial Value
The initial value of the step tag or sequencing parameter. This value is assigned to the
Value
field when the
Equipment Sequence
is initialized. Initialization occurs when the
Equipment Sequence
is commanded to START, RESET, or both. Step tag and sequencing parameter initial values are editable. Sequence Parameters control validates the value so it is within the configured Min and Max range.
Initialize as Valid
Indicates whether the step output tag or sequencing output parameter value is valid or invalid on initialization of the
Equipment Sequence
.
Expression
Defines an expression that is evaluated to a value for step input tags and sequencing output parameters.
Data Type
Displays the data type of the step tag or sequencing parameter. Data types for step tags and sequencing parameters include SEQ_DINT, SEQ_SINT, SEQ_INT, SEQ_REAL, SEQ_BOOL, and SEQ_STRING.
Description
Displays the text entered to describe the tag or parameter. Description text is optional and can be blank.
Engineering Unit
Displays the text entered to describe the engineering unit.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal