Command a transition using the Sequence Detail Control
You can force an active transition to evaluate TRUE, STOPPING and RESETTING the preceding steps while attaching and STARTING these steps.
TIP:
The
Equipment Sequence
must be in Automatic
mode.Before you begin
- Open a display that contains the Sequence Detail Control.
- TheEquipment Sequenceshould be RUNNING.
- The transition must be active.
To command a transition using the
Equipment Sequence
Monitor- SelectTake Ownership
to take ownership of the
Equipment Sequence. - Select on the active transition.
- SelectForce Transition
to force the expression to TRUE
. - When finished, selectRelease Ownership
.
Provide Feedback