Sequence Detail Control events

The
Sequence Detail Control
has these events that can be used by a client in runtime.
Event
Description
ActiveStepCountChanged
Event indicates that the count of active steps in the displayed
Equipment Sequence
has changed. The event has a single integer parameter that is the ActiveStepsCount property value.
AutoScrollChanged
Event occurs whenever the value of the AutoScroll property changes. The event has a single Boolean parameter that is the current AutoScroll property value.
FailedStepCountChanged
Event indicates that the count of failed steps in the displayed
Equipment Sequence
has changed. The event has a single integer parameter that is the FailedStepsCount property value.
StepSelectionChanged
Event occurs when the value of the SelectedStepName property changes. The event has a single string parameter that is the SelectedStepName property value.
everyTagConnectedChanged
Occurs whenever the value of the IsEveryTagConnected property changes. The event has a single bool parameter that is the current IsEveryTagConnected property value.
liveDataConnectedChanged
Occurs whenever the value of the IsLiveDataConnected property changes. The event has a single bool parameter that is the current IsLiveDataConnected property value.
seqMgrServerConnectedChanged
Occurs whenever the value of the IsSeqMgrServerConnected property changes. The event has a single bool parameter that is the current IsSeqMgrServerConnected property value.
seqMgrServerConnectedBackupChanged
Occurs whenever the value of the IsSeqMgrServerConnectedBackup property changes. The event has a single bool parameter that is the current IsSeqMgrServerConnectedBackup property value.
seqMgrServerToControllerConnectedChanged
Occurs whenever the value of the IsSeqMgrServerToControllerConnected property changes. The event has a single bool parameter that is the current IsSeqMgrServerToControllerConnected property value.
seqMgrServerToControllerConnectedBackupChanged
Occurs whenever the value of the IsSeqMgrServerToControllerConnectedBackup property changes. The event has a single bool parameter that is the current IsSeqMgrServerToControllerConnectedBackup property value.
sequenceStateChanged
Occurs whenever the value of the SequenceState property changes. The event has a single integer parameter that is the current SequenceState property value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal