Sequence Summary Control columns in the table area

These columns are displayed in the
Equipment Sequence
list in the table area of the Sequence Summary Control. The list can be sorted in alphabetical order for any column to group
Equipment Sequence
s based on status.
Status column
Description
Sequence Name
The
Equipment Sequence
name.
ID
The identifier assigned to the
Equipment Sequence
before it runs. This field is editable when the sequence is inactive, or in the IDLE state. When the sequence is active, the ID field is locked.
State
The current execution state of the
Equipment Sequence
. Possible states include NOT CONNECTED, IDLE, RESTARTING, RUNNING, RESETTING, HOLDING, STOPPING, ABORTING, HELD, STOPPED, ABORTED, and COMPLETE.
Mode
The operational mode for the
Equipment Sequence
, either
Automatic
, in which sequence steps advance automatically, or
Manual
, in which the operator advances sequence steps manually.
Phase Failure
Indicates a failure in an
Equipment Phase
associated with the sequence.
Sequence Failure
Indicates a failure in the
Equipment Sequence
.
Owners
The current owner of the
Equipment Sequence
.
Unit ID
A numerical representation of the piece of equipment that the
Equipment Sequence
is controlling.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal