Perform basic functions

Basic functions for the application on the HMI device include logging on and off, entering data, opening a screen, interacting with a popup, selecting a graphic element, triggering an action, and viewing diagnostic messages. The configuration of the application determines the interactions to perform on the HMI device.
Perform basic functions on the HMI device to interact with the contents of the application.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal