Use the runtime application
The runtime application is downloaded to an HMI device for interaction at runtime. Each runtime application has its own look and feel based on its configuration in
Studio 5000
View Designer
. Using the data configuration and application created in Studio 5000
View Designer
, the HMI device screen animates the contents of the project by responding to data values from the controller. If configured, the screen responds to touch and keys. Use the runtime application to interact with screens and data and to perform system operations.
Provide Feedback