PDF Viewer
On the HMI device, an example PDF_Viewer_Landscape includes:

Item | Description | |
![]() | Bookmarks for the PDF document in the PDF_Viewer_Landscape. | |
![]() | Bookmarks displays the bookmarks of the PDF document. To display bookmarks, configure bookmarks for the PDF before adding the PDF to the View Designer project. | |
![]() | Previous opens the previous page in the PDF document. If there is no previous page to open, the button appears unavailable. | |
![]() | Next opens the next page in the PDF document. When on the last page, the button appears unavailable. | |
![]() | The open page in the PDF document. Specify a different page number to open a different page in the PDF document. | |
![]() | The name of the PDF document in the PDF Viewer. | |
![]() | Fit Width expands the width of the PDF document to the width of the PDF Viewer. | |
![]() | Fit Window expands the size of the PDF document to the size of the PDF Viewer. | |
![]() | Zoom In increases the PDF document magnification by the percentage specified in the event command. | |
![]() | Zoom Out decreases the PDF document magnification by the percentage specified in the event command. | |
![]() | The PDF document specified for the PDF Viewer. In View Designer , the PDF document must exist in the Documents folder of the Project Explorer . | |
Provide Feedback