Create an Add-On Graphic

Create an Add-On Graphic to create a custom graphic element. Add-On Graphics are empty by default. Add graphic elements to the definition of an Add-On Graphic like any other other screen or popup.
View Designer
does not allow adding another Add-On Graphic to the definition of an Add-On Graphic.
To create an Add-On Graphic
  1. In the
    Project Explorer
    , expand the
    Assets
    folder.
  2. Right-click the
    Add-On Graphics
    folder and select
    New Add-On Graphic
    . An initial Add-On Graphic named
    AddOnGraphic_001
    appears.
  3. Type a new name for the Add-On Graphic:
    • The name must not exist for another Add-On Graphic in the
      Add-On Graphics
      folder.
    • The name must contain only numbers, letters, and underscores.
  4. The name must not begin with a number, contain spaces, have more than one underscore in a row, or end with an underscore. Press
    Enter
    .
    TIP:
    • Add-On Graphics appear alphabetically in the
      Add-On Graphics
      folder in the
      Project Explorer
      . Renaming or deleting the
      Add-On Graphics
      folder from the
      Project Explorer
      is not allowed.
    • Properties for the definition of the Add-On Graphic appear in the
      Properties
      window.
    • Add-On Graphics appear in the
      Toolbox
      in the
      Add-On Graphics
      category.
    • To add content to an Add-On Graphic, double-click to open the Add-On Graphic, and then add graphic elements to the definition of the Add-On Graphic as if it were any other screen.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal