Predefined Add-On Graphics
Predefined Add-On Graphics exist in the
Add-On Graphics
folder under Assets
in the Project Explorer
. These Add-On Graphics display, zoom, and navigate PDF documents on the HMI device: - PDF_Viewer.Occupies the entire screen of a six-inch or nine-inch HMI device.
- PDF_Viewer_Landscape.Occupies the entire screen of a 10-inch HMI device and a portion of larger HMI devices. The PDF_Viewer_Landscape Add-On Graphic is not available on six-inch or nine-inch HMI devices.
- PDF_Viewer_Portrait.Occupies half of the screen of an HMI device. The PDF_Viewer_Portrait Add-On Graphic is not available on six-inch or nine-inch HMI devices.
Provide Feedback