Reuse of images in an Add-On Graphic between projects

If the copied definition of the Add-On Graphic contains an image that already exists in the target project, replace the image in the target project or cancel.
Copying the definition of an Add-On Graphic that has an image file that already exists in the target project, but with a different image, adds an increment number to the name of the image in the target project. For example, if copying the definition of an Add-On Graphic that has an image named Tank1 and that image contains tank.bmp, and the target project also has an image file named Tank1 but that image contains watertank.bmp, the name of the image in the target project is incremented to Tank1_001.
Not replacing an image in the Add-On Graphic in the target project copies the Add-On Graphic to the target project, but an empty image appears on the canvas of the definition of the Add-On Graphic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal