Rename an Add-On Graphic
Rename an Add-On Graphic when the definition or purpose of the Add-On Graphic changes. For example, if an Add-On Graphic with a single tank for a beverage line now contains two tanks, change the name from Single_Tank to Double_Tank. Changing the name of an Add-On Graphic does not break the link to any instances of the Add-On Graphic.
To rename an Add-On Graphic
- In theProject Explorer, expand theAssetsandAdd-On Graphicsfolders and then navigate to select the Add-On Graphic.
- Select the Add-On Graphic to select the item.
- Select the item again and type the new name.TIP:Tips:
- Rename an Add-On Graphic by right-clicking the name and selectingRename. Then type a new name and pressEnter.
- To rename the Add-On Graphic, type a new name in theNamebox of thePropertieswindow.
- The name must not exist for another Add-On Graphic in the Add-On Graphics folder.
- PressEnter.
Provide Feedback