Change the property values for the definition of an Add-On Graphic

Change the property values for the definition of an Add-On Graphic. All properties for the definition of an Add-On Graphic are optional.
To change the property values for the definition of an Add-On Graphic
  1. If the definition of the Add-On Graphic is open, select the background of the Add-On Graphic.
  2. In the
    Properties
    window, change the property values.
    TIP:
    In the
    Project Explorer
    , expand the
    Assets
    and
    Add-On Graphics
    folders to navigate to and select the
    Add-On Graphic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal