Delete an Add-On Graphic from a project

Delete an Add-On Graphic from a project to no longer add it to a screen or popup. It is not possible to undelete an Add-On Graphic.
Prerequisites
  • Delete all instances of the Add-On Graphic in the project. If the Add-On Graphic is used in the open project, it appears in the
    Graphic Explorer
    .
To delete an Add-On Graphic from a project
  1. In the Project Explorer, open the
    Assets
    and
    Add-On Graphics
    folders to navigate to the Add-On Graphic.
  2. Right-click the Add-On Graphic and select
    Delete
    . The Add-On Graphic is removed from the project.
    TIP:
    If the Add-On Graphic is currently used in the project, a warning message appears indicated that the Add-On Graphic cannot be deleted. Delete all instances of the Add-On Graphic in the project and then delete the Add-On Graphic from the
    Project Explorer
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal