Change the vendor of an Add-On Graphic

Change the vendor of an Add-On Graphic to change the name of the company that owns the Add-On Graphic.
To change the vendor of an Add-On Graphic
    1. In the
      Project Explorer
      , expand the
      Assets
      and
      Add-On Graphics
      folders to navigate to and select the Add-On Graphic.
    TIP:
    If the definition of the Add-On Graphic is open, you can select the background of the Add-On Graphic.
    In the
    Properties
    window, expand the
    General
    category.
  1. In the
    Vendor
    box, type the name of the company that owns the Add-On Graphic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal