Enter data using a physical keyboard

Use the external physical keyboard to enter data.
  1. Select the screen or graphic element requiring numeric input.
  2. Enter data as required.
  3. Press Enter to confirm and submit the data.
    TIP:
    Tips:
    • If you enter data into an element and change the focus before pressing Enter, the data is discarded.
    • When entering a value using the numeric input or text input elements, the Value or Text property of the element that is bound to a controller does not receive updates until you press Enter to send the value to the controller and exit the inline edit mode.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal