Navigate and zoom a PDF document
Navigate a PDF document on the HMI device. The buttons and functionality available on the HMI device depend on the configuration of the PDF graphic element or the PDF Viewer Add-On Graphic.
TIP:
The
PanelView
5310 HMI device does not support the PDF Viewer graphic element or the PDF Viewer Add-On Graphic. To navigate or zoom a PDF document
- Select a button to navigate the PDF document:
- Bookmarks
displays the bookmarks. - Previous
opens the previous page. - Next
opens the next page. - Page Numberopens the page of the PDF document entered in thePage Numberbox.
- Fit Width
expands the width of the PDF document. - Fit Window
expands the entire page of the PDF document to fit the PDF graphic element. - Zoom In
increases the PDF document magnification by the percentage specified in the ByPercent property of the Zoom In event command. - Zoom Out
decreases the PDF document magnification by the percentage specified in the ByPercent property of the Zoom In event command.TIP:Tips:- PDF files that contain complex drawings take longer to render. For example, if a PDF contains an image that is actually a drawing of individual shapes such as lines, circles, and rectangles, that image takes longer to render than a drawing that is a single image.
- On a keypad terminal, press a key to navigate the pages of a PDF document:
- Home: Navigate to the first page.
- End: Navigate to the last page
- Page Up: Navigate to the previous page.
- Page Down: Navigate to the previous page.
- Up, Down, Right, and Left arrows: Navigate the content of the displayed page.
Provide Feedback