Open a screen
Open any screen that is accessible with the assigned security rights. When opening a screen, an overlay dims the current screen to show interaction with the screen is not available. When the new screen opens, interaction with the screen is available immediately. Interact with the new screen when the overlay from the previous screen still appears or when the new screen is loading content. By default, the
Home
screen of the project opens on the HMI device. To open a screen
- On the HMI device or in theSystem Bannerat the top of the screen, selectNavigation
. The Navigation menuopens. - Select to open a:
- Screen.Select the item in theNavigation menu.
- Home screen.SelectHome
in the Navigation menu. - Next screen.SelectNext
in the System Bannerto open the next screen in navigation history. - Previous screen.SelectPrevious
in the System Bannerto open the previous screen in navigation history. - Folder.Select a folder in theNavigation menuto display screens within the folder. The contents of the folder appears in an upper row. Folders may contain subfolders. Breadcrumbs shows the current folder path in the upper row.
- Previous folder.SelectBack
to the left of the breadcrumbs to navigate back a folder. TIP:Tips:- Using an external keyboard, tab to the item and pressEnter.
- When using an external keyboard, use the following keys to navigate theNavigation menu:
- Next item.Press the right arrow andEnter.
- Previous item.Press the left arrow andEnter.
- First item.PressHomeandEnter.
- Last item.PressEndand pressEnter.
- Next page of menu items.PressPage Down.
- Previous page of menu items.PressPage Up.
Provide Feedback