View error messages for a graphic element
A graphic element or group of graphic elements in error is outlined in red and has an
. An
appears for 10 seconds for any graphic element that has an event with a command that is in error. Select this icon to open an
Error
icon
. An Error
icon
appears for 10 seconds for any graphic element that has an event with a command that is in error. Select this icon to open an Error list
with the diagnostic messages associated with a graphic element in error. If an error occurs for any property of a graphic element, the properties that set position, size, and angle freeze. When the properties of the graphic element are no longer in error, the last written values for the position, size, and angle properties apply to the graphic element.
To view diagnostic messages for a graphic element in error
- Select theErroricon
on the graphic element or tabto highlight the icon and pressEnter. TheError listopens. - View the errors and diagnostic messages for the graphic element:Graphic elementActionCurrent graphic element
- Swipe vertically or select theDown ArrowandUp Arrowat the bottom and top of theError listto scroll the error messages.
- Using an external keyboard, press theDown ArrowandUp Arrowkeys to scroll to the next and previous line of error messages.
- Using the physical keypad, pressPage Down
and Page Up
to scroll to the next page of error messages. - PressHome
and End
to go to first or last line of the error messages.
Next graphic element in a group of graphic elements in error- Swipe horizontally from right to left, or select theRight Arrowin the lower right corner of theError list. The diagnostic messages for the next graphic element in error appear in theError list.
- Using the physical keypad on the HMI device or an external keyboard, pressTab
to highlight the button and press Enter. - Using the physical keypad on the HMI device or an external keyboard, press theRight Arrowkey.
Previous graphic element in a group of graphic elements in error- Swipe horizontally from left to right, or select theLeft Arrowin the lower right corner of theError list. The diagnostic messages for the previous graphic element in error appear in theError list.
- Using the physical keypad on the HMI device or an external keyboard, pressTab
to highlight the button and press Enter. - Using the physical keypad on the HMI device or an external keyboard, press theLeft Arrowkey.
- To close theError list, selectClose
. Using the physical keypad on the HMI device or an external keyboard, press Esc.TIP:Closing theError listmakes theErroricon
disappear.
Provide Feedback