Interact with a popup
Interact with a popup by opening, moving, or closing the popup. To identify the event that opens a popup, contact the HMI Designer.
To interact with a popup
- Perform the event to open the popup. For example, select a button configured with a press event configured inStudio 5000View Designer.
- Perform any action required by the popup. If theVirtual Standard KeyboardorVirtual Numeric Keypadopens, enter the required data. Popup contents may include events and animations. Interacting with a popup may perform an event or animation depending on the configuration of the popup. Selecting a button on the popup may change the appearance of the button.
- To close a popup, selectClose
on the popup or select elsewhere on the screen.TIP:Tips:- To move a popup, select and drag the caption at the top of the popup.
- Move a portion of a popup off the edge of the HMI device screen to provide more room on the screen.
- Only popups with captions can move.
- Opening another popup or theNavigation menucloses the open popup.
- Performing an event may close a popup. To identify events configured for the application, contact the HMI Designer.
Provide Feedback