Enter data using the Virtual Numeric Keypad
Use the
Virtual Numeric Keypad
to enter data. Touching the screen or graphic element requiring numeric input opens the Virtual Numeric Keypad
. The minimum and maximum values to enter for the selected element appear below the Input
box on the Virtual Numeric Keypad
. To enter data using the Virtual Numeric Keypad
- Touch the screen or graphic element requiring numeric input. TheVirtual Numeric Keypadopens. Any value for the element appears highlighted in theInputbox at the top of the keypad.
- Enter or change the data:
- Select the keys to enter the numeric value.
- SelectPositive-Negative Value
to toggle the number in the Inputbox between a positive and negative number. - SelectBackspace
to delete one number to the left at a time. - To remove all of the numbers in theInputbox, selectClear
.
- To enter the value, selectOK. To close theVirtual Numeric Keypadand not enter the value, selectCancelor elsewhere on the screen.TIP:Tips:
- A red outline appears around theInputbox for an incorrect entry.
- To enter a value using an external keyboard, tab to highlight the first key on theVirtual Numeric Keypad, select the arrow keys to highlight a key,and then pressEnter.
Provide Feedback