Remove media from the HMI device

Prepare the SD card for safe removal from the HMI device so that the files on the SD card do not become corrupt.
To remove the SD card from the HMI device
  • Perform the event configured with a
    Safely Remove Media
    command. To identify events to perform, contact the HMI Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal