Select a graphic element
Touch a graphic element to select it or use the HMI device keypad or an external keyboard. Placing focus on a graphic element using the HMI device keypad or an external keyboard places a highlighted rectangle around the graphic element.
Touching a graphic element or selecting a graphic element with an external keyboard and pressing
Enter
may trigger an event. To learn configured events, contact the HMI Designer. To select a graphic element
- Select the desired graphic element on a screen, popup, orSystem Banner. Any configured event for the graphic element triggers.TIP:Tips:
- If a graphic element in error appears off or near an edge of the screen, an arrow with anErroricon
points in the direction of the graphic element. Select the arrow to open the Error listfor the graphic element. - To select a graphic element using the HMI keypad or an external keyboard, select or pressTaborBack Taband then select or pressEnter.
- Using an external keyboard, pressShift+Tabto back tab.
- If selectingTaborBack Tabdoes not select a graphic element, it highlights the first or last item on the screen that accepts focus.
- If an item in theSystem Banneris highlighted, selectingTaborBack Tabhighlights the next or previous selectable item in theSystem Banner.
- Tabbing and back tabbing highlights graphic elements on the screen and theSystem Banner.
- Tabbing and back tabbing within a popup highlights graphic elements within the popup only.
Provide Feedback