Create an object

Create an object

Create an object to add the node to
Project view
.
  1. In
    Project view
    , select the folder to create the object and then select
    Add new
    in the
    Project view
    toolbar, or right-click the folder and select
    New
    .
  2. Select
    Object
    or the specific object. 
ObjectName1
appears in
Project view
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal