Create linear gauges
Create linear gauges that enable you to view and control specific motor configuration settings.
TIP:
The gauges duplicate the functionality of the spin boxes in the default recipes editor widget.
- Create max RPM gauge:
- InProject view, right-clickMainWindow (type)and select
- Hover-over the gauge, select, and enter
EditMaxRPMGauge. - InProperties, create a dynamic link between theValueproperty and .For more information about dynamic links, see Create dynamic links.
- Create max RPM label:
- InProject view, right-clickMainWindow (type)and select
- Hover-over the gauge, select, and enter
EditMaxRPMLabel. - InProperties, setTexttoMax RPM.
- Create min throttle gauge:
- InProject view, right-clickMainWindow (type)and select
- Hover-over the gauge, select, and enter
EditMinThrottleGauge. - InProperties, create a dynamic link between theValueproperty and .For more information about dynamic links, see Create dynamic links.
- Create min throttle label:
- InProject view, right-clickMainWindow (type)and select .
- Hover-over the gauge, select, and enter
EditMinThrottleLabel. - InProperties, setTexttoMin Throttle.
Provide Feedback