Configure network interface settings
Configure the network interface to create the network interface and name the interface type.
- InProject view, expand the object and select theSystemobject.
- InProperties, next toNetwork interfaces, select
NetworkInterface.NetworkInterfaceappears in#Propertieswith settings to display and edit at runtime. - InInterface name, enter an interface type exactly as it appears inFactoryTalk Optix System Manager.
- LAN
- WAN
- Wi-Fi
- If required, configure the network properties:
- DHCP activated. Enable or disable automatic IP address assignment in DHCP mode.
- IP address. Primary IP address.
- Mask. Subnetwork mask.
- DNS 1. DNS1 IP address. For WAN and Wi-Fi interfaces only.
- DNS 2. DNS2 IP address. For WAN and Wi-Fi interfaces only.
- Gateway. Default gateway IP address.
- Additional IP addresses. Additional IP addresses of the interface. For Lan interface only.
Provide Feedback