Properties pane
Use the
Properties
pane to display variables for the selected object. Property values change the appearance and display of that object at runtime. The Properties
pane also displays Events
for the selected object. An event is something that occurs to trigger an action called a method. Events initiate on the HMI device in runtime.
Item | Description | Function |
|---|---|---|
![]() | Group by category | Organize the properties by category. |
![]() | Sort alphabetically | Sort the properties in alphabetical order. |
![]() | Add new | Add a property to the node. Add a display name, variable, alias, or audit signature. In the Events category of the Properties pane, this button adds a new event from the Events header or a new method for the selected event. |
Delete | Remove an added property from the Properties pane or reset the value of a default property. In the Events category of the Properties pane, this button deletes the selected method. Removing all methods from an added event deletes the event. | |
![]() | Open with editor | Open the editor for the selected object. This button is valid for only certain object types. |
Provide Feedback