Assign a group to a user
Use
Manage Users and Groups
to assign groups and create a hierarchy of rights and privileges.- In the main toolbar, either:
- Select
Open dashboard page, and then on the dashboard, selectI want to manage users and groups. - Select the drop-down arrow after
Open dashboard page, and then selectManage users and groups.
- InManage Users and Groups, either:
- From underGroups,drag a group onto a user or hold downShiftorCtrlto select and drag consecutive or multiple groups to a user.
- Select the checkbox of one or more groups, selectAssigngroups to users, select the checkbox of a user, and then selectApply.
appears next to a user that is already assigned to a group. - SelectExit.
- Select
Save.InManage users and groups, you can drag a user into a group.
Provide Feedback