System object configuration
Depending on your system requirements, you may want to configure the
System
object as well as the DateTimeConfiguration
and WiFiConfiguration
objects. The properties for these objects override the
FactoryTalk Optix System Manager
at runtime.Object | Properties |
|---|---|
System | LAN and WAN network interface settings |
System.DateTimeConfiguration | System Date, Time, and Time zone. Set these properties manually or through a remote NTP server. |
System.WiFiConfiguration | WAN, LAN, and Wi-Fi network interface settings |
You can manually configure graphic components and logics. For example, link the
DHCP enabled
property to the Active
property of a switch. At runtime, network interface properties are automatically added to the
System
object using the FactoryTalk Optix System Manager
configuration to display the current settings. For example, if a system has a LAN network interface that is configured with two additional IP addresses, at runtime, the System
object contains a Network interface
object for the LAN network and a collection of Additional IP addresses
with two additional IP addresses.Provide Feedback