Create a button that shuts down the host system
Add a button that shuts down the host operating system on which the
FactoryTalk Optix Application
runs.
IMPORTANT:
Pressing
Shut down system
immediately shuts down the host operating system
on which the FactoryTalk Optix Application
runs.For example, if you run the
FactoryTalk Optix Application
on an emulator target, pressing Shut down system
immediately shuts down your Windows system.- InProject viewpane, right-clickMainWindow (type)and select .
- Hover-over the button, select, and enter
EditShutDownSystemButton. - InProperties, setTexttoSHUT DOWN HOST SYSTEM.
- InEvents, next toMouseClick event, selectand select .
Add
Provide Feedback