Create a thermometer linear gauge
Create a linear gage with a warning zone that indicates the current temperature.
- Create and configure the gauge:
- Right-clickMainWindow (Type)and select .
- Hover-over a gauge, select, and enter
EditThermometerGauge. - InProperties, create a dynamic link betweenValueand .For more information about dynamic links, see Create dynamic links.
- Set the value gauge warning zone:
- InProperties, next toWarning zones, select.
Add - UnderWarningZone1, setColorto#f30000.
- SetFromto75.
- SetToto100.
Provide Feedback