Debug NetLogic

Identify, investigate, and fix issues with NetLogic code by locally using Visual Studio or Visual Studio Code.
To debug NetLogic remotely, see Debug runtime NetLogic remotely.
TIP: NetLogic errors are reported at runtime in the
FactoryTalk Optix Studio
log panel. NetLogic runtime errors are reported in the tab of the target on which the application runs (for example, ). The design-time NetLogic errors are reported in the tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal