Configure the Network Configurator widget
Configure the
Network Configurator
widget to display and edit the Settings for WAN, LAN, and WiFi network interfaces.Prerequisites
To configure the Network Configurator widget
- Select
Template Libraries. - InLibraries, selectWidgets.
- UnderComponents, dragNetwork ConfiguratorintoProject view.
- InLibraries, selectClose.
- InProject view, expandNetworkConfiguratorDialog(type)to displayPropertiesfor the type.
- Drag theSystemobject to#SystemNodeinProperties.The system settings are associated with the widget.
- At runtime, perform the desired edits, and then selectApply.
Provide Feedback