Set the unit of measure for a variable

Set the unit of measure for a variable

Set the unit of measurement for a numeric figure.
  1. In
    Project
    view
    , select the variable.
  2. In
    Properties
    , right-click the numeric value and select
    New > EUInformation
    .
  3. In the
    EUInformation
    Editor
    , select the unit of measure for the variable and choose
    Select
    .
The unit of measure appears in the value for the variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal