Create a motor object
Create a motor object and motor configuration to use it in a recipe.
- Create a motor object
- InProject view, right-clickModeland select .
- Hover-over the object, select, and enter
EditMotor - Add and configure variables:
- InProperties, at the top, add two variables by selectingand selecting
AddVariable. - Rename the variables by hovering-over each variable, selecting, and entering:
Edit- Speed
- Acceleration
- Create a motor configuration object
- InProject view, right-clickMotorand select .
- Hover-over the object, select, and enter
EditConfiguration - Add and configure variables:
- InProperties, at the top, add three variables by selectingand selecting
AddVariable. - Rename the variables by hovering-over each variable, selecting, and entering:
Edit- MaxRevolutionsPerMinute
- MaxThrottle
- MinThrottle
Provide Feedback