Remove a unit of measure from a variable

Remove a unit of measure from a variable

Remove the unit of measure for a variable to no longer have the value for that variable appear in that unit of measure.
  1. In
    Project
    view
    , select the variable.
  2. In
    Properties
    , in the value for the variable, select the unit of measure.
  3. In the
    EUInformation Editor
    , select the unit of measure and select
    Delete
    .
  4. Select
    OK
    .
The unit of measure is removed from the variable.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal