Close a project
Close a project from the Start page.
You can have more than one project open at a time. When you open additional projecjts, additional instances of
FactoryTalk Optix Studio
open.
- From the main toolbar, select
Project. On the Start page, selectClose.
TIP:
If you open the Start page from an open project and want to close the Start page, select
.
. Provide Feedback