Develop a user management interface

Develop a user management interface

Develop a multilingual user management solution from scratch.
TIP: Instead of creating the user management interface from scratch, you can use the predefined widgets. For more information, from the toolbar, select Template Libraries and search for
User Editor
The user management interface enables you to:
  • Create user accounts
  • Remove user accounts
  • Change the password and location of user accounts
Application example
TIP:
You can download a sample project from:
UserManagementInterface.zip
Prerequisites
In
FactoryTalk Optix Studio
, select
Run
Run
to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal