Arrange graphic objects

After you draw or paste objects, you can move them around and arrange them using the menu options on the Arrange menu or the toolbar. You can:
  • Stack objects by moving them in front of or behind other objects.
  • Align objects with each other or vertically or horizontally.
  • Space objects vertically or horizontally.
  • Flip objects horizontally or vertically.
  • Rotate objects around an anchor point.
  • Combine several objects into a group that behaves as a single object.
  • Separate a grouped object into its component objects.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal